FLEXCOMM Pins of LPC55S69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FLEXCOMM Pins of LPC55S69

ソリューションへジャンプ
2,267件の閲覧回数
SrinathVelavan
Contributor III

I am working on creating a custom device with LPC55S69 as Host MCU. For a peripheral that is interfaced with LPC55S69 on SPI interface, I have used Flexcomm 1 (Pins 13 & 14) as MOSI & MISO respectively and Flexcomm 3 ( Pin 7) for SSEL. Can we use 2 different Flexcomm interfaces (1 & 3) for the same peripheral or should all pins be in the same Flexcomm interface?? 

#lpc55s69

0 件の賞賛
返信
1 解決策
2,231件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

All SPI signals must routed to the same Flexcomm instance.

Hope it helps you.

Have a nice day!

元の投稿で解決策を見る

2 返答(返信)
2,232件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

All SPI signals must routed to the same Flexcomm instance.

Hope it helps you.

Have a nice day!

2,210件の閲覧回数
SrinathVelavan
Contributor III

Thank you for your clarification. Will make the necessary changes 

タグ(1)
0 件の賞賛
返信