FLEXCOMM_GetInstance crashing (HS SPI)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FLEXCOMM_GetInstance crashing (HS SPI)

3,726 次查看
christianlees
Contributor III

I have a board using a LPC55S06 and a Winbond W25Q32 connected to the HS SPI interface.

	CLOCK_SetClkDiv(kCLOCK_DivFrohfClk, 0U, true);  /*!< Reset FROHFDIV divider counter and halt it */
	CLOCK_SetClkDiv(kCLOCK_DivFrohfClk, 2U, false); /*!< Set FROHFDIV divider to value 2 */
	CLOCK_AttachClk(kFRO_HF_DIV_to_HSLSPI); /*!< Switch HSLSPI to FRO_HF_DIV */
	//CLOCK_AttachClk(kMAIN_CLK_to_HSLSPI);
	RESET_PeripheralReset(kHSLSPI_RST_SHIFT_RSTn);

	spi_master_config_t master_config = {0};
	SPI_MasterGetDefaultConfig(&master_config);
	master_config.sselNum = (spi_ssel_t)0;
	master_config.sselPol = (spi_spol_t)kSPI_SpolActiveAllLow;
	master_config.baudRate_Bps = 12000000U;
	uint32_t clk = CLOCK_GetHsLspiClkFreq();
	SPI_MasterInit(SPI8, &master_config, CLOCK_GetHsLspiClkFreq());

 

Stepping through the code the MCU crashes when it returns from FLEXCOMM_GetInstance.  I have tried a few difference baud rates.

uint32_t FLEXCOMM_GetInstance(void *base)
{
    uint32_t i;
    pvoid_to_u32_t BaseAddr;
    BaseAddr.pvoid = base;

    for (i = 0U; i < (uint32_t)FSL_FEATURE_SOC_FLEXCOMM_COUNT; i++)
    {
        if (BaseAddr.u32 == s_flexcommBaseAddrs[i])
        {
            break;
        }
    }

    assert(i < (uint32_t)FSL_FEATURE_SOC_FLEXCOMM_COUNT);
    return i;
}

 

When this routine runs i is 8 as is FSL_FEATURE_SOC_FLEXCOMM_COUNT when it gets to the assert line.  If i step into this line I get the following line in the debugger console

[Inferior 1 (Remote target) exited normally]

Any idea what causes this?

0 项奖励
回复
4 回复数

3,703 次查看
christianlees
Contributor III

According to the user manual (UM11424) the HS_SPI is on Flexcomm 8 (SPI8), page 622.  Is this different between the two packages?

Christian

0 项奖励
回复

3,694 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you refer to data sheet rather than user manual, the user manual only gives function description for all the family, the data sheet gives how many modules the processor has exactly for each derivative.

Sorry for the discrepancy between user manual and data sheet.

BR

XiangJun Rong

0 项奖励
回复

3,689 次查看
christianlees
Contributor III

The pin tool in the development environment lists  flexcomm 0 - 6 and 8.  Inside Flexcomm 8 the options are all for HS SPI and the pin numbers look correct.

3,715 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the data sheet of LPC550x.

For HTQFP64 pins of LPC550x, there are only 6 spi plus 1 hs spi, total is 7

For HTQFP48 pins of LPC550x, there are only 3 spi plus 1 hs spi, total is 4

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1637131180985.png

 

0 项奖励
回复