FDI-LPC3250-Ethernet Diconnecting Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FDI-LPC3250-Ethernet Diconnecting Issue

1,018件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pradeep Kumar on Wed Jan 08 06:30:32 MST 2014
Hi,

I am using LPC-3250 custom board ported with kernel 2.6.34.For file system mounting i'm using ramdiskboot and mtdboot procedures.When the board is getting powered in that time ethernet is connected properly and i'm running applications on board .But after some time in both the booting procedure  ethernet getting disconnected. In H/W side on board ICS1893AFI IC is mounted for ethernet interfacing.

  The following dmesgs are getting when i'm using ramdiskboot procedure

   nfs: server 192.168.1.10 not responding, still trying

How can i recetify this issue on LPC3250.Can any one suggest me to get out of this issue.


Thanks In Adv &  Regards,


Pradeep Kumar G.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)