External SDRAM bank selection on LPC407x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

External SDRAM bank selection on LPC407x

跳至解决方案
2,174 次查看
otavioborges
Contributor III

Hello,

I'm currently developing an application using LPC4078FBD208 that will use 3 external AS4C4M16S SDRAM ICs from Alliance.

I've been following AN10950 to perform connections between SDRAM and MCU. Example from Fig. 5 on the AN is the most similar with my SDRAM IC pinout. But I have a question on the Address Bus.

I noticed that MCU pins EMC_A[0:23] have been connected to memory address bus and the two bank pins to EMC_A13 and EMC_A14.

My doubt exactly is why EMC_A12 was skipped (A11 from SDRAM is connected to EMC_A11 but BA0 was connected to EMC_A13). There's a particular reason from that? This example is for LPC24XX family but is directly applicable to LPC407x family?

标签 (1)
1 解答
2,014 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Otavio,

You must use A13 and A14 instead of A12 and A13. The LPC4088 always uses A13/A14 to output the bank select signals, independent of the SDRAM memory organization. Yes, you can use the application note as reference for your design.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

在原帖中查看解决方案

1 回复
2,015 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Otavio,

You must use A13 and A14 instead of A12 and A13. The LPC4088 always uses A13/A14 to output the bank select signals, independent of the SDRAM memory organization. Yes, you can use the application note as reference for your design.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer