Example of set LPC4370 Base_M4_Clock to 204MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example of set LPC4370 Base_M4_Clock to 204MHz

1,342 Views
cpchen
Contributor III

Dear Sir, 

Is there code example of how to set the Base_M4_Clock to 204Mhz ?  from the power on default 96MHz .

I have read through se. 13.2 of LPC4370 user manual, and understand the procedures, but I would very appreciate to have a working code example that I can learn from. 

Best Regards,

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,219 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi CP chen,

   Please refer to our LPCopen code, I have test the LPC4370 lpcopen code, that project already configure the clock to 204Mhz, this is the test result:

pastedImage_1.png

You can find the lpcopen code from this link:

LPCOpen Software for LPC43XX|NXP 


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply