Example Projects for LPC1102

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example Projects for LPC1102

1,262 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Handler on Thu Jul 18 03:29:11 MST 2013
Hello,

I cannot download examples for 1102 from this page  :tired: :
http://www.lpcware.com/content/project/nxp-peripherals/usb-nxp-microcontrollers/lpcxpresso-support
Links just don't work.

I need:
LPCXpresso Blinky Example Project for LPC1102 with ISP V1.0 (May 16, 2011)
LPCXpresso Systick Example Project for LPC1102 V1.0 (May 19, 2011)

Could you please give me correct link or may be upload  this projects to this forum.

Thanks.
Labels (1)
0 Kudos
Reply
1 Reply

1,228 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 18 07:39:20 MST 2013
There are a couple of ZIP files with examples specifically for the LPC1102 and LPC1104 in the Examples subdirectory of your LPCXpresso IDE installation:

C:\nxp\LPCXpresso_5.2.6_2137\lpcxpresso\Examples\NXP\LPC1000\LPC1102_LPC1104

Note that in reality the only real change between LPC11xx and LPC1102/1104 examples is that the CMSISv2p00_LPC1102 library project sets the clock
up to use the IRC Oscillator in system_LPC11xx.c. This has been done as the LPCXpresso1102/1104 boards do not make use of an external crystal.

Thus generally you can make use of any code aimed at the LPC11xx family.

Regards,
LPCXpresso Support
0 Kudos
Reply