Ethernet using LPCXpresso LPC1769 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet using LPCXpresso LPC1769 board

842 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leandro.stlima on Wed Jan 08 09:14:23 MST 2014
Hi fellows,

I am having a problem programming to get the data from Ethernet with LPCXPresso Board 1769. I have the same code running ok with another board using the same microprocessor but with Embedded Artist's board the code doesn't work. I can see that leds from ethernet chip work fine but there's no data coming.

I'm using the EMAC example from Micromint Lincoln e60 board and it's based on uIP code. It seems to me that this code is almost the same to the LPC board.

Has someone any idea about it? Knows this problem?

Thanks
Labels (1)
0 Kudos
Reply
0 Replies