Ethernet socket programming on lpc43s50fet256 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet socket programming on lpc43s50fet256 processor

1,492 次查看
sulomulo
Contributor I

I want to make ethernet connection to my lpc43s50fet256 microprocessor .I will connect lan8710 tranciever  at24c02 eeprom .I dont know how to code my  processor pins to achieve this.

标记 (3)
0 项奖励
回复
1 回复

1,246 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer could refer OM13027 board schematics about how to connect LPC43xx with LAN8720 Ethernet PHY.

The AT24C02 EEPROM is using I2C bus, which also refer below circuit as an example:

pastedImage_1.png

pastedImage_2.png

The I2C bus pull up resistor value could be 10K or 4.7K as required.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复