Ethernet interface on 100 pin LPC4370

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet interface on 100 pin LPC4370

1,237件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Sun Jan 05 08:01:37 MST 2014
Hi mc,

This is a follow-on to the earlier thread which would accept the new submission?

I still think the full Ethernet interface does not exist on the 100 pin LPC4370?

For instance, the port P9 which would contain ENET_RXD3 at P9_2 is apparently not implemented on the 100 pin version?

Please confirm whether the full Ethernet interface is implemented on this device - a current project depends on its availability.

Thanks for your response.

JohnR
ラベル(1)
0 件の賞賛
返信
1 返信

1,193件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Jan 09 15:21:50 MST 2014
Answer is at below link

http://www.lpcware.com/content/forum/ethernet-lpc4370fet256fet100
0 件の賞賛
返信