Ethernet bootloader for LPC1833

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet bootloader for LPC1833

1,136件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mohcinen on Tue Jul 15 05:50:37 MST 2014


Hi,
I'm looking for an ethernet bootloader for LPC1833 without success.
Is this bootloader exist? if not is it planned?
Best regards,
Mohcine
ラベル(1)
0 件の賞賛
返信
1 返信

1,105件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Fri Aug 08 06:00:18 MST 2014
There is nothing planned from NXP side. The bootloader in LPC1833 is like it is, it is in true ROM and can't be changed or updated without creating a new chip version.
The LPC1833 can boot from internal flash, qSPI or external flash directly, so in one of these memories there must be an ethernet application which is acting as a secondary bootloader. In principle this is already application level.
One or the other ethernet example in our LPCOpen package can maybe be used as a template to write this "firmware-download-via-ethernet" application.

Regards,
NXP Support Team
0 件の賞賛
返信