Ethernet bootloader for LPC1833

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet bootloader for LPC1833

1,135 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mohcinen on Tue Jul 15 05:50:37 MST 2014


Hi,
I'm looking for an ethernet bootloader for LPC1833 without success.
Is this bootloader exist? if not is it planned?
Best regards,
Mohcine
Labels (1)
0 Kudos
Reply
1 Reply

1,104 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Fri Aug 08 06:00:18 MST 2014
There is nothing planned from NXP side. The bootloader in LPC1833 is like it is, it is in true ROM and can't be changed or updated without creating a new chip version.
The LPC1833 can boot from internal flash, qSPI or external flash directly, so in one of these memories there must be an ethernet application which is acting as a secondary bootloader. In principle this is already application level.
One or the other ethernet example in our LPCOpen package can maybe be used as a template to write this "firmware-download-via-ethernet" application.

Regards,
NXP Support Team
0 Kudos
Reply