Ethernet Tutorial

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Tutorial

1,094 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mfarnet on Thu Aug 01 09:09:19 MST 2013
Can someone point me to an application note or tutorial that describes how to get the EMAC interface up and running?  I'm looking for basic stuff to take us through EMAC initialization, PHY initialization, then basic packet transfer and then on to TCP/IP (LWIP or uIP).  And then Telnet or HTTP server.

It would be nice to understand the flow of data so that the knowledge can be used to change target hardware and still know what the heck is happening rather than blindly applying reference designs and demo software packages.

Thanks,

Mike.
Labels (1)
0 Kudos
Reply
0 Replies