Ethernet Communication Between Two LPC2478 Boards Using Internal SRAM (Broadcast Mode, LPCXpresso ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Communication Between Two LPC2478 Boards Using Internal SRAM (Broadcast Mode, LPCXpresso ID

1,160 Views
VijayaJangam1
Contributor II

I'm working on Ethernet communication between two LPC2478 boards using LPCXpresso IDE. I want to send a string from one board to another using broadcast MAC (FF:FF:FF:FF:FF:FF) and store all buffers in internal SRAM (no external RAM or lwIP). send data in the form string from transmitter to receiver Give me corrections and why this problem face.

0 Kudos
Reply
1 Reply

1,091 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @VijayaJangam1 

It seems this question is the same as the one posted at this link. My colleague will reply to you in that thread.

Thank you.

 

BR

Alice

 

0 Kudos
Reply