Error when importing lpcopen_v2_00a_lpcxpresso_nxp_lpcxpresso_11u14.zip and lpcopen_2_05_lpcxpresso_nxp_lpcxpresso_1343.zip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when importing lpcopen_v2_00a_lpcxpresso_nxp_lpcxpresso_11u14.zip and lpcopen_2_05_lpcxpresso_nxp_lpcxpresso_1343.zip

2,377 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glerm on Fri Aug 29 07:58:12 MST 2014
The following error is displayed when trying to import pcopen_v2_00a_lpcxpresso_nxp_lpcxpresso_11u14.zip and lpcopen_2_05_lpcxpresso_nxp_lpcxpresso_1343.zip

Have attached the error screen.

Using Ubuntu 12.04 LTS with LPCXpresso v7.3.0 [Build 186] [2014-07-09]

Can someone suggest a fix please?

Georg



Labels (1)
0 Kudos
Reply
10 Replies

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glerm on Sat Aug 30 04:43:38 MST 2014
- can you try importing other projects into the same workspace (other LPCOpen projects, or Examples supplied in the project). What happens?
[color=#00f]Problem still occurs[/color]
- can you try creating a new (empty) workspace and then importing these failing projects into it. What happens?
[color=#00f]Problem still occurs[/color]
If your projects still do not import, finally,
- can you try deleting the .eclipse directory in your home directory. Repeat the steps above. What happens?
[color=#00f]Problem still occurs[/color]

I Have removed LPCXpresso v7.3.0 and installed LPCXpresso v7.2.0 , and was able to install both the files with no problems, as well as the ones that worked.

For now I will use LPCXpresso v7.2.0

Thank you very much for your help.

Georg
0 Kudos
Reply

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat Aug 30 01:00:05 MST 2014
Sorry, but I can't explain this. Some further questions/things to try (in order)
- can you try importing other projects into the same workspace (other LPCOpen projects, or Examples supplied in the project). What happens?
- can you try creating a new (empty) workspace and then importing these failing projects into it. What happens?
If your projects still do not import, finally,
- can you try deleting the .eclipse directory in your home directory. Repeat the steps above. What happens?
0 Kudos
Reply

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glerm on Fri Aug 29 11:23:54 MST 2014
I have reinstalled LPCXpresso, and still have the same problem.

Any other ideas?
0 Kudos
Reply

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Aug 29 09:04:29 MST 2014
That actually looks like an internal database corruption in your LPCXpresso installation. I suggest you uninstall and re-install.

0 Kudos
Reply

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glerm on Fri Aug 29 08:52:20 MST 2014
I have downloaded them twice. Do have an alternate download location available?

I have used the download link http://www.lpcware.com/system/files/lpcopen_v2_00a_lpcxpresso_nxp_lpcxpresso_11u14.zip and http://www.lpcware.com/system/files/lpcopen_2_05_lpcxpresso_nxp_lpcxpresso_1343.zip.



Thank you for your help thus far.
0 Kudos
Reply

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glerm on Fri Aug 29 08:45:03 MST 2014
Not using "Import from XML description"

.log attached (renamed to .log.txt)
0 Kudos
Reply

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Aug 29 08:42:22 MST 2014
BTW: I have just downloaded and imported both of these projects and they work as expected. The only other thing I can suggest is that your downloaded zip files are corrupted. Download them again.
0 Kudos
Reply

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Aug 29 08:36:15 MST 2014
It looks like you are using "Import from XML description" - as the error is being reported in the XML parser.

If you are not doing that, please zip and attach the flle
[your_workspace]/.metadata/.log
0 Kudos
Reply

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glerm on Fri Aug 29 08:21:08 MST 2014
Thank you for the quick response.

I am using the import in the quickstart panel as per your suggestion.
I have successfully imported the other lpcopen files which are lpcopen_2_01_lpcxpresso_nxp_lpcxpresso_812.zip and lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769.zip
Sorry for not mentioning that in original post.

0 Kudos
Reply

2,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Aug 29 08:04:20 MST 2014
How are you trying to import? To import these projects you should use
Quickstart panel
  Import projects...
And then use the Browse button in the Project archive group.

This is described in the User Guide.
0 Kudos
Reply