Error on MCUXPresso Config Tool: FLEXCOMM driver NOT found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error on MCUXPresso Config Tool: FLEXCOMM driver NOT found

6,498件の閲覧回数
misterbee
Contributor II

So I created a base project based on SDK example freertos_hello using the online SDK builder. I choose GNU toolchains. I build and run on target so far so good.

 

But then I want to move on configuring I2C using the MCUXpresso Config tool from the project. I turn on the peripheral and add the FLEXCOM1 into peripheral as I want to use it for I2C. But then I have this error:

"Issue: FLEXCOMM Driver not found in the toolchain/IDE project. Project will not compile!
Level: Error
Type: Validation
Tool: Toolchain/IDE project
Origin: Peripherals
Target: Toolchain/IDE project: cm4
Resource: platform.drivers.flexcomm_i2c"

. How should I resolve this? Is there anyway I can add this I2C driver from the Config tools itself?

 

0 件の賞賛
返信
7 返答(返信)

6,488件の閲覧回数
misterbee
Contributor II

I am using development board LPC54114

 

misterbee_0-1656067946392.png

 

0 件の賞賛
返信

6,473件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have tried to configure the I2C with FlexComm0 module, for the error, pls put the mouse  on the error message which is located at  the right-bottom of the peripheral menu, then right click the mouse, update the software file, the error will disappear.

BTW, I suppose that you can refer to the I2C example code, then copy the code to your application based on freeRtos, including pin configuration, clock configuration.

xiangjun_rong_0-1656311034862.png

Hope it can help you

BR

XiangJun Rong

6,058件の閲覧回数
PedroBecerra
Contributor III
This solved my problem too.
LPADC Driver not found in the toolchain/IDE project. Project will not compile!
0 件の賞賛
返信

6,464件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the screenshot to fix the error message.

xiangjun_rong_0-1656494125487.png

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

6,360件の閲覧回数
misterbee
Contributor II

Thank you @xiangjun_rong , what did you do to show that option?

In my case, I did right click on the problem row and just showing this, no option to add driver from SDK

 

misterbee_0-1658909854195.png

 

0 件の賞賛
返信

6,470件の閲覧回数
misterbee
Contributor II

Thank you @xiangjun_rong ,

 It seems your snapshot is using MCUXPresso IDE But I am using GNU tool chains. Can' I resolve this without switching the toolchains? I hope so.

0 件の賞賛
返信

6,490件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the part number so that we can have a check?

BR

XiangJun Rong

0 件の賞賛
返信