Error in final launch sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in final launch sequence

3,912件の閲覧回数
hazemselmi
Contributor II

I am using LPC1769 board and LPCxpresso IDE.

When I click debug, it ends with error message:

Error in final launch sequence
Error: Error reported by server (redlinkserv.exe):
Status fail.

Note:

I am using 15 lpc1769 board (for teaching purposes), all of them work fine (using the same code and same USB cable) except 3 boards that give me some problems.

ラベル(1)
4 返答(返信)

3,729件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

See Regaining debug access to target MCU

Thanks and regards,

MCUXpresso Support

3,729件の閲覧回数
hazemselmi
Contributor II

Thanks for the reply.

This worked for two boards.

However few still have some problem.

The error is:

Error in final launch sequence
Error: Error reported by server (redlinkserv.exe):
Status fail
LinkServer has been terminated and will be restarted.
Please restart your debug session.

(Also I noted that some ICs in lpc-link became extremely hot). 

0 件の賞賛
返信

3,729件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

It sounds like you're using the older NXP LPCXpresso1769 Rev. B boards. The LPCXpresso1769 Rev. D use CMSIS-DAP, and the debug circuit is different. In both cases, power is supplied to the LPC1769 through the debug circuit. If any IC in this circuit is hot to the touch, it suggests a hardware problem. Possibly due to static damage which is common in a classroom environment. Sorry we can't help further.

Thanks and regards,

MCUXpresso Support

0 件の賞賛
返信

3,729件の閲覧回数
hazemselmi
Contributor II

I understand, and believe you are right! (Some boards have a hardware problem).

BUT, what about this error:

02: Failed on connect
02: Failed on connect
Target marked as not debuggable.
Emu(0): Connected. Was: None. DpID: EDB6. Info: HID64HS12

and

Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm3_nxp -msg-port=54784 -g -mi -2 -pLPC1769 -vendor=NXP -vc -e0 -wire=hid -flash-driver=LPC175x_6x_512.cfx
Error message from debugger back end:
Remote communication error. Target disconnected.: No error.
Remote communication error. Target disconnected.: No error.

0 件の賞賛
返信