Error in User Manual LPC4357 - Rev. 1.9 - Feb 2015

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in User Manual LPC4357 - Rev. 1.9 - Feb 2015

1,164件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Wed Jun 24 02:43:37 MST 2015
Page 1248 - Description of Bit TXIE (Bit 11):

11 TXIE Transmit interrupt enable 0 R/W
0 The INTPND bit will be left unchanged after a
successful reception of a frame.
1 INTPND will be set after a successful reception
of a frame.

Description of value 0 and 1 tells something about "reception", but I think must be "transmission"...
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,155件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Wed Jul 01 14:30:33 MST 2015
"Page 1256:
When the configuration is completed, MSAGVALis set to valid again."

seems also to be broken (typo).

On same page there is bit TXRQUT, which is never mentioned anywhere else.
0 件の賞賛
返信

1,154件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Wed Jun 24 08:45:46 MST 2015
Hi capiman,

That certainly does not look right. I will let the documentation team know. Thank you for finding this error!
0 件の賞賛
返信