Error: Flash Download failed - "Cortex-M0+"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error: Flash Download failed - "Cortex-M0+"

12,489件の閲覧回数
vidhya1
Contributor III


Hello Sir,

Previously LPC845 sample codes were executing correctly,
I had tested blinky code on LPCXpresso845MAX board, but
after I updated the pack installer, I'm not able to load
the file to MCU board, erase can be done but not able to load.

When checked the error in google, it directed to keil site,
where I need to download the LPC845 pack http://www.keil.com/dd2/pack/
But i'm not able to install it.

Kindly guide me how to resolve this issue.

ラベル(1)
3 返答(返信)

11,630件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To address the issue, I'd like to know more information, so I was wondering if you can answer the following question.
1. What's the version of the Keil you use?
2. Whether you can install the pack of LPC845 in the Pack Installer.

pastedImage_1.png
3. Whether you can share the screenshot of the download error

Have a great day.

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

11,625件の閲覧回数
vidhya1
Contributor III

Thanks for the reply sir.

1. What's the version of the Keil you use?

I'm using Keil U vision 5.24

2. Whether you can install the pack of LPC845 in the Pack Installer.

https://community.nxp.com/servlet/JiveServlet/downloadImage/2-1119302-255964/pastedImage_1.png

IMAGE 1 ATTACHED - BUT IN TARGET UTILITIES OPTION THERE IS NO MCU PART

FOUND

IMAGE 2 ATTACHED - INSTALLED IMAGE OF LPC845

3. Whether you can share the screenshot of the download error

Please find the attached images of error when I'm loading to MCU.

BUILD COMPILE1 IMAGE - BUILD COMPILE ERROR

ERROR 1 IMAGE - CANNOT FLASH ERROR

ERROR 2 IMAGE - Error: Flash Download failed - "Cortex-M0+"

Previously it was working fine sir, when I updated pack installer again,

i'm not able

load the program to MCU.

Kindly advice.

Thanks & Regards,

Vidhya

0 件の賞賛
返信

11,625件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
According to the attachments, this issue is raised by missing the FLM file.
Whether you can check the FLM file exist in the path(~/Keil_v/ARM/PACK/NXP/LPC845_DFP/11.0.0/arm), if not, give a try reinstall the pack after removing LPC845's pack.

845.png

Have a great day.

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------