Error: Flash Download failed - Target DLL has been cancelled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error: Flash Download failed - Target DLL has been cancelled

2,813 次查看
swamy1
Contributor I

Hello,

I am using Jlik to program LPC2148 in keil software. I am getting this error please help to overcome with this issue.

Thanks and regards,

Thippeswamy H Uerror_jlink.png

0 项奖励
回复
1 回复

2,684 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Have you been able to connect with the target at least once? You should verify the following:

  1. Target processor is properly powered.
  2. Debug connector from J-Link to target processor is properly mapped, oriented and connected.
  3. The PC have installed the drivers for J-Link debugger.
  4. Keil project configuration is properly set for the desired memory, included the related Flash driver file.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复