Erasing MCU after enabling secure boot in LPC55S16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Erasing MCU after enabling secure boot in LPC55S16

1,811 Views
nxf64834
NXP Employee
NXP Employee

Hi all,

Can we mass erase the chip using blhost after enabling secure boot in LPC55S16 ?

If no, then the chip will get scrapped if incorrect data is programmed?

Is there any document with list of commands that are allowed in blhost after enabling secure boot?

Labels (1)
0 Kudos
Reply
1 Reply

1,798 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

If you want to change configuration, you can program the empty CMPA into chip.

Recommend have a look at:

https://www.nxp.com.cn/docs/en/application-note/AN12283.pdf 

0 Kudos
Reply