Erasing LPC1833 internal EEPROM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Erasing LPC1833 internal EEPROM

跳至解决方案
2,716 次查看
michaelershov
Contributor I

Hello,

I am using the LPC1833 and the internal EEPROM. I'm not understand,does EEPROM erase, when erasing Flash with programmer, or the only way to use erasing from my code? It's generally a part of Flash memory or not?

Best regards

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,356 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

It really depends on the Flash programmer.  Fundamentally, Flash and EEPROM are separate peripherals with different programming interfaces. Actions performed to one will have no effect on the other.

LPCScrypt can be used to program and erase EEPROM and also supports an erase all command - this simply calls the erase function of all programmable devices known to LPCScrypt on a particular MCU.

Also LPCOpen provides example code to manage the programming of EEPROMs.

Yours,

LPCXpresso-support

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,356 次查看
michaelershov
Contributor I

Ok, and if I store important information in EEPROM; Flash protected from reading. Anyone can erase only Flash and write new code for reading EEPROM?

Best regards

0 项奖励
回复
2,357 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

It really depends on the Flash programmer.  Fundamentally, Flash and EEPROM are separate peripherals with different programming interfaces. Actions performed to one will have no effect on the other.

LPCScrypt can be used to program and erase EEPROM and also supports an erase all command - this simply calls the erase function of all programmable devices known to LPCScrypt on a particular MCU.

Also LPCOpen provides example code to manage the programming of EEPROMs.

Yours,

LPCXpresso-support

0 项奖励
回复