Erase EEPROM with debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Erase EEPROM with debugger

2,467 Views
eddwhite1
Contributor I

Hello,

Is it possible to erase the EEPROM of an LPC4078 using the debugger (either J-Link or LPC-Link 2)?

Labels (2)
0 Kudos
Reply
2 Replies

2,343 Views
soledad
NXP Employee
NXP Employee

Hi,

You need to use IAP commands.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,222 Views
Sahil_Bhat
Contributor II

Hi, 

I am new to IAP commands.

Where can I find IAP command to erase the EEPROM of LPC4078 device? Where/How can I execute that command? Please advise.

 

Thanks

Sahil

0 Kudos
Reply