Enquiry about the interrupt event setting training notes or tutorials

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enquiry about the interrupt event setting training notes or tutorials

4,006 Views
jhtan
Contributor I

Hi, may i know is this link (Session 6: Interrupts - NXP Community) still available?

Could anyone pls share the training notes or tutorials about the LPC MCU interrupt event setting?

0 Kudos
Reply
5 Replies

3,980 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, unfortunately, the video is not available, but could you let me know what board you are using? the example on the SDK does not have the name interrupt they call PIT.

Pavel_Hernandez_0-1697065307346.png

Best regards,
Pavel

 

0 Kudos
Reply

3,964 Views
jhtan
Contributor I

Hi.

I have try the lpadc_interrupt example of LPC55s28, may i know how to set this SDK into high resolution mode? As i notice the full range print out is only 4096.

0 Kudos
Reply

3,969 Views
jhtan
Contributor I
Hi Pavel, i am using LPC MCU (55s28, 55s36) and RT1170 MCU as well.
It will be great if you have any video tutorial regarding the interrupt setting for these few boards.
0 Kudos
Reply

3,975 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The SDK provides the Pin interrupt example in SDK as Pavel pointed out.

I attach the user guide of Cortex-M4, pls read the NVIC chapter, it is helpful to understand the interrupt mechanism for ARM mcu.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply

3,969 Views
jhtan
Contributor I
Hi, Thx a lot for the support. May i know is there any interrupt mechanism differences for cortex m33 and m4?
0 Kudos
Reply