EmWin Transparent Button with Bitmap Image ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EmWin Transparent Button with Bitmap Image ?

4,059 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tonko on Fri Dec 13 02:37:22 MST 2013
  Hi !

I'm trying to use bitmap image on Button widget. Only bitmap image on button should be visible, button should be transparent.
Part of bmp image is transparent and I want to see background window around button image where image is transparent.
What is wrong now is that button is visible in background, It should be transparent or invisible.

Source files in attachment

Original Attachment has been moved to: Button_AdvancedSettings64x64.c.zip

Original Attachment has been moved to: WindowDLG.c.zip

标签 (1)
0 项奖励
回复
2 回复数

2,638 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Cusko on Fri Dec 20 04:57:14 MST 2013
Look at the attachment. Try if it works for you.
0 项奖励
回复

2,638 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ildar on Fri Dec 13 04:16:06 MST 2013
Hello!

We solved same problem with method:
  
    
#define GUI_INVALID_COLOR0xFFFFFFF      /* Invalid color - more than 24 bits */

...
GUI_Init();
BUTTON_SetDefaultSkin(Custom_BUTTON_DrawSkinFlex);
...

static int Custom_BUTTON_DrawSkinFlex(const WIDGET_ITEM_DRAW_INFO * pDrawItemInfo)
{
switch (pDrawItemInfo->Cmd)
{
case WIDGET_ITEM_DRAW_BACKGROUND:
{
GUI_COLOR background = BUTTON_GetBkColor(pDrawItemInfo->hWin, BUTTON_CI_UNPRESSED);
if (background != GUI_INVALID_COLOR)
{
return BUTTON_DrawSkinFlex(pDrawItemInfo);
}
break;
}
default:
return BUTTON_DrawSkinFlex(pDrawItemInfo);
}
return 0;
}


With regards, Gilmanov Ildar
0 项奖励
回复