EmWin 5.18 crash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EmWin 5.18 crash

1,525件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by luc.vercruysse on Mon Oct 06 14:43:51 MST 2014
My system crashes after QUI_init(). When I do not call the SysTick_Config function all works fine.
It seems that the interrupt jumps to a undefined location. When I do not use EmWin library, the sys_tick interrupt is handled OK.

Any idea ??

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,469件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by luc.vercruysse on Tue Oct 07 08:33:46 MST 2014
No problems with 5.24. Thanks for response !
0 件の賞賛
返信

1,469件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Oct 06 23:41:50 MST 2014
Try a later release? Nxp are shipping 5.24 now.
http://www.lpcware.com/content/project/emwin-graphics-library
0 件の賞賛
返信