EmWin 5.18 crash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EmWin 5.18 crash

1,532 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by luc.vercruysse on Mon Oct 06 14:43:51 MST 2014
My system crashes after QUI_init(). When I do not call the SysTick_Config function all works fine.
It seems that the interrupt jumps to a undefined location. When I do not use EmWin library, the sys_tick interrupt is handled OK.

Any idea ??

Labels (1)
0 Kudos
Reply
2 Replies

1,476 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by luc.vercruysse on Tue Oct 07 08:33:46 MST 2014
No problems with 5.24. Thanks for response !
0 Kudos
Reply

1,476 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Oct 06 23:41:50 MST 2014
Try a later release? Nxp are shipping 5.24 now.
http://www.lpcware.com/content/project/emwin-graphics-library
0 Kudos
Reply