Ef(34): Timed-out initializing flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ef(34): Timed-out initializing flash

2,703 Views
lhlonng
Contributor I

Hi:

    MCU: LPC54018
    BOARD: LPCXpresso540xx Eval Brd Rev E

    Problem: can't program the flash,the error log from MCXpresso IDE is:

    "chip initialization failed - Ef(34): Timed-out initializing flash.

    failed to initialize flash driver LPC540xx_SPIFI_SFDP.cfx"

    the eval board can run the demo download before which compiled by myself.

    how can i fix it?

0 Kudos
Reply
3 Replies

2,696 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Please show your steps how to download and debug your project?

Also first use a SDK demo to test.

 

BR

Alice

0 Kudos
Reply

2,685 Views
lhlonng
Contributor I

Hi:

steps:

   1. open mcuxpresso ide

    2. install SDK_2.8.2_LPCXpresso54018-OM13790DOCK.zip

    3. import lpcxpresso54018_om13790dock_usb_pd_alt_mode_dp_dock_bm

    4. compile

    5. install JP5 install,JP2 is fitted in position 1-2,not install JP1

    6. connect  to connector J8 with micro USB cable

    7. click GUI Flash tool 

    8. click MCUxpresso IDE LinkServer

    9. click run in the window of  GUI Flash Tool

    10. click confirm to download

    11. IDE indicate that flash init fail

0 Kudos
Reply

2,672 Views
Alice_Yang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply