EMC configuration and calibration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EMC configuration and calibration

1,732 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hiromi on Fri Mar 08 04:34:17 MST 2013
Hello, I'm using a PSRAM to run code and I need to improve the performance.

Microcontroller: lpc1788.
PSRAM: IS66WVE2M16BLL.
Clock: 96MHz

EMC configuration:
LPC_SC->EMCCLKSEL = 0;
LPC_EMC->Control = 0x00000001;enabled...            
LPC_EMC->Config  = 0x00000000;
EMC_StaMemConfigMW(2,EMC_StaticConfig_MW_16BITS);
EMC_StaMemConfigPB(2,EMC_StaticConfig_PB);
WAITWEN (NS_2_CLKS(24)));
WAITOEN (NS_2_CLKS(0)));
WAITRD (NS_2_CLKS(70)));
WAITPAGE (NS_2_CLKS(20)));
WAITWR (NS_2_CLKS(46)));
WAITTURN(0x01));
delay();
pageMode();
bufferEnable();


QUESTION 1:

I read in the User Manual that EMC can be calibrated using EMCCAL.

With this code I obtain the calibration value:

  LPC_SC->EMCCAL |= EMC_CAL_START;
  while(!(LPC_SC->EMCCAL & EMC_CAL_DONE));
  uint32_t calibrationValue = EMC_CAL_CALVALUE(LPC_SC->EMCCAL);

But I don't know how to use this value.

In the UM it is suggested to "Adjust one or more programmable delays if needed based on the calibration result."

How should I use the calibration value to adjust the EMC delays?

QUESTION 2:

How should I configure the following:
  LPC_SC->EMCDLYCTL =     
    EMC_DLYCTL_CMDDLY(x)| // x * 250ps
    EMC_DLYCTL_FBCLKDLY(y)|
    EMC_DLYCTL_CLKOUT0DLY(z)|
    EMC_DLYCTL_CLKOUT1DLY(k);?

Thank You in advance...
Labels (1)
0 Kudos
Reply
2 Replies

1,674 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Mon Mar 18 09:12:24 MST 2013
EMC Calibration is for SDRAM....
0 Kudos
Reply

1,674 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hiromi on Mon Mar 11 05:19:06 MST 2013
Really nobody can help me please?
0 Kudos
Reply