EMC boot pin configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EMC boot pin configuration

1,290 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sh on Thu Nov 21 04:12:18 MST 2013
Hi all,

When using EMC 16-bit boot mode, I observe that contrary to what is written in UM10503 V1.7 Chapter 5.3.6.2, address pins which are actively driven are A0..A20, and the remaining address pins are configured for passive pull-up rather than pull-down. I am not using a header in my image. The board I am trying this with is an old Hitex LPC4350 eval board (version A2).

I haven't found anything in the errata that would explain this discrepancy between chip and documentation.

The NOR flash chip used on the Hitex board has a capacity of 4 MByte and thus needs A21. The fact that this pin is being passively pulled up instead of pulled down upsets the booting process.

Am I doing something wrong, is the documentatiuon wrong, or is it a bug in the LPC4350 boot ROM?

Cheers
Labels (1)
0 Kudos
Reply
1 Reply

1,270 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sh on Thu Nov 21 14:41:30 MST 2013
I am replying to myself with some new information.

The behavior I described above was with the debugger (LPCXpresso) downloading and starting the image. When the ROM bootloader starts the image, without debugger intervention, it initializes address lines up to A14 (not A13 as described in the manual), and the others are initialized for passive pulldown.

I don't know why the debugger does things differently (and still wrong). It just makes it harder to figure out what happens. As it stands, the ROM boot code and the debugger disagree with each other, and with the documentation in the processor manual.

When booting from external parallel flash, one needs to make sure that all the code and read-only data is in the first few kilobytes of flash, that gets accessed before the pin muxing is set up correctly. In LPCopen, I can see nothing that makes sure this is the case. The SystemInit function is called before initialization of static/global variables is done, but neither the SystemInit function nor the various chip library functions it calls are put in a special section, so they can end up almost anywhere in the image, depending on the linking order. If perchance they end up too far away from the beginning of the image: Crash.

If anyone would elect to put the stack into external memory, it would be even worse, since the startup code would have to set up pin muxing and EMC configuration without using the stack, which precludes calling a function, and requires a few special attributes on the ResetISR function. Clearly, LPCopen is not even remotely able to cope with that in its current form. I guess it would require to convert SystemInit into a macro that does not use any real function calls, and contains only code that works with the registers.
0 Kudos
Reply