EMC StaticMem for nor flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EMC StaticMem for nor flash

1,383件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Badman on Wed Apr 23 08:46:22 MST 2014
I have an example for LPC4088, which uses memory flash S29GL064 for Keil. Ported it to the LPCXpresso but the lack of data read from memory. Field variables NOR_ID always have a value 65535.
Why below code works compiled in Keil, but not LPCXpresso ?
#include "emc_nor.h"
#include "lpc_timer.h"
 
/* Private define ------------------------------------------------------------*/
#define NOR_FLASH_START_ADDR       ((uint32_t)0x90000000)
#define NOR_FLASH_END_ADDR         ((uint32_t)0x90800000)
 
/* Delay definition */   
#define SectorErase_Timeout        ((uint32_t)0x00A00000)
#define ChipErase_Timeout          ((uint32_t)0x30000000) 
#define Program_Timeout            ((uint32_t)0x00001400)
 
#define ADDR_SHIFT(A)              (NOR_FLASH_START_ADDR + (2 * (A)))
#define NOR_WRITE(Address, Data)   (*(volatile short *)(Address) = (Data))
 
typedef struct
{
  uint16_t Manufacturer_Code;
  uint16_t Device_Code1;
  uint16_t Device_Code2;
  uint16_t Device_Code3;
}
NOR_IDTypeDef;
 
NOR_IDTypeDef NOR_ID;
 
/*******************************************************************************
* Function Name  : EMC_NOR_Init
* Description    : Configures the FSMC and GPIOs to interface with the NOR memory.
*                  This function must be called before any write/read operation
*                  on the NOR.
* Input          : None
* Output         : None
* Return         : None
* Attention : None
*******************************************************************************/
void EMC_NOR_Init(void)
{
TIM_TIMERCFG_Type TIM_ConfigStruct;
EMC_STATIC_MEM_Config_Type config;
 
/**************************************************************************
* Initialize EMC for NOR FLASH
**************************************************************************/
config.CSn = 1;
config.AddressMirror = 0;
config.ByteLane = 1;
config.DataWidth = 16;
config.ExtendedWait = 0;
config.PageMode = 0;
config.WaitWEn = 2;
config.WaitOEn = 2;
config.WaitWr = 0x1f;
config.WaitPage = 0x1f;
config.WaitRd = 0x1f;
config.WaitTurn = 0x1f;
StaticMem_Init(&config);
 
    // init timer
TIM_ConfigStruct.PrescaleOption = TIM_PRESCALE_USVAL;
TIM_ConfigStruct.PrescaleValue= 1;
 
// Set configuration for Tim_config and Tim_MatchConfig
TIM_Init(LPC_TIM0, TIM_TIMER_MODE,&TIM_ConfigStruct);
TIM_Waitms(100);
 
//delay time
 TIM_Waitms(10);
 
  return;
}
 
/******************************************************************************
* Function Name  : EMC_NOR_ReadID
* Description    : Reads NOR memory's Manufacturer and Device Code.
* Input          : - NOR_ID: pointer to a NOR_IDTypeDef structure which will hold
*                    the Manufacturer and Device Code.
* Output         : None
* Return         : None
* Attention : None
*******************************************************************************/
void EMC_NOR_ReadID(NOR_IDTypeDef* NOR_ID)
{
  NOR_WRITE(ADDR_SHIFT(0x0555), 0x00AA);
  NOR_WRITE(ADDR_SHIFT(0x02AA), 0x0055);
  NOR_WRITE(ADDR_SHIFT(0x0555), 0x0090);
 
  NOR_ID->Manufacturer_Code = *(volatile short *) ADDR_SHIFT(0x0000);
  NOR_ID->Device_Code1 = *(volatile short *) ADDR_SHIFT(0x0001);
  NOR_ID->Device_Code2 = *(volatile short *) ADDR_SHIFT(0x000E);
  NOR_ID->Device_Code3 = *(volatile short *) ADDR_SHIFT(0x000F);
}
 
/******************************************************************************
* Function Name  : EMC_NOR_ReturnToReadMode
* Description    : Returns the NOR memory to Read mode.
* Input          : None
* Output         : None
* Return         : NOR_SUCCESS
* Attention : None
*******************************************************************************/
NOR_Status EMC_NOR_ReturnToReadMode(void)
{
  NOR_WRITE(NOR_FLASH_START_ADDR, 0x00F0);
 
  return (NOR_SUCCESS);
}
void main (void)
{ 
  uint32_t index;
  uint16_t sector;
  uint8_t nor_error;
 
  /* Initialize the FSMC NOR Flash Interface */
  EMC_NOR_Init();
  /* Set the NOR read modes */
  EMC_NOR_ReturnToReadMode();
 
  EMC_NOR_ReadID(&NOR_ID);
 
  while(1)
  {
  }
}


ラベル(1)
0 件の賞賛
返信
1 返信

1,260件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Badman on Thu May 01 10:39:31 MST 2014
Problem solved. I forgot to set the bit EMCS in the register SCS:
LPC_SC->SCS |= (1<<0);
0 件の賞賛
返信