EMC_D5 vs SD_DAT3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EMC_D5 vs SD_DAT3

1,006 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Heikon on Tue Dec 04 03:29:35 MST 2012
as I tried to config the port and pins for our application I got the problem,
that EMC_D5 and SD_DAT3 are on the same Pin and no other configuration is possible.
did I overlooked something or can I only use one of those interfaces?
thanks
heiko
Labels (1)
0 Kudos
Reply
1 Reply

996 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DF9DQ on Tue Dec 04 03:44:59 MST 2012
That is the unfortunate truth. Only the LBGA256 package can use external memory and wide SD card bus together, but none of the smaller packages. :-(

Regards,
Rolf
0 Kudos
Reply