EEPROM in LPC54608

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEPROM in LPC54608

3,503件の閲覧回数
TEMCEFF
Contributor IV

I have gone through the user manual of LPC54608 regarding EEPROM. In that they mentioned, writing of EEPROM required two steps: They are:

The first step is writing a minimum of 1 word (4 bytes) to a maximum of 32 words (128 bytes)
to the desired page in the 16 kB EEPROM address space at address 0x4010 8000.

Step two is an erase/program of that page into non-volatile memory.

I don't understand that meaning.

and I have seen the SDK files. In that also, data reading from EEPROM is also not available.

Thanks and Regards,

Avinash.

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

3,490件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

I will gladly answer your questions. Step one refers to write the data in the address you chose. The data will be at the address but it won't be written in the memory until you program it in step 2.

nxf54944_1-1609356813236.png

You cannot read the data when you are on step 1, to read the data you need to have the data programmed in the memory.

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

 

 

 

0 件の賞賛
返信

3,482件の閲覧回数
TEMCEFF
Contributor IV

can you provide step by code for my reference and why it is taking two steps to store data.

0 件の賞賛
返信

3,464件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

An EEPROM device cannot be programmed directly, that's why writing data to it and erase/program of the memory are two different steps.

You can find EEPROM examples at the SDK https://mcuxpresso.nxp.com/en/welcome

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

0 件の賞賛
返信