EEPROM NXH5104 sample source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EEPROM NXH5104 sample source code

3,275 Views
haulam
Contributor II

I'm going to use EEPROM NXH5104 in my product . 

Do we have any sample source code which implement the read/write function of this chip ?

0 Kudos
Reply
4 Replies

2,921 Views
Carlos_Mendoza
NXP Employee
NXP Employee


Hi Hau Lam,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

2,921 Views
haulam
Contributor II

Hi @Carlos, Any update on this topic ? Thank you very much.

0 Kudos
Reply

2,921 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Hau Lam,

 

Apologies for the delay, I see that the NXH5104 EEPROM is a SPI device so I would recommend you use the perich_ssp example that comes with the LPC11C24 LPCOpen package for more information on how to send information through SPI:

LPCOpen Software for LPC11XX|NXP 

 

Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

2,921 Views
haulam
Contributor II

Hi Carlos,

I'm using MCU LPC1115.

0 Kudos
Reply