EA's 7" LCD interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EA's 7" LCD interface

3,097件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by e135193 on Sat Aug 04 15:56:38 MST 2012
Hello

    Does EA's 7" LCD has an extra SPI configuration pin ?

    I come accross code line like below. I guess that these bunch of code is required to initialize the LCD. As I trying to find the datasheet of the EA's 7" LCD. I found attached LCD datasheet which does not have an extra SPI pins.

    Does any one have the datasheet of EA's 7" LCD ? Or is the one that I found correct ?

    I'm trying to change the emWin 5.16 code for my 7" LCD which do not have an SPI interface. Does someone help ?

   

Engin
   


static void _InitTrulyLCD(void) {
  //
  // Power LCD
  //
  LPC_GPIO2->DIR |= 1;  // Set to output
  LPC_GPIO2->SET  = 1;  // Output LCD power
  //
  // Set display CMD/DATA register select pin to output high
  //
  LPC_GPIO0->DIR |= (1 << LCD_REG_BIT);
  //
  // Display init sequence
  //
  _WriteLcdReg(0x00,0x0001);
  _DelayMs(15 * 2);
  _WriteLcdReg(0x03,0x6E3E);  // AAAC
  _WriteLcdReg(0x0C,0x0007);  // 0002
  _WriteLcdReg(0x0D,0x000E);  // 000A
  _WriteLcdReg(0x0E,0x2C00);  // 2C00
  _WriteLcdReg(0x1E,0x00AE);  // 00B8
  _DelayMs(15 * 2);

  _WriteLcdReg(0x07,0x0021);
  _DelayMs(50 * 2);
  _WriteLcdReg(0x07,0x0023);
  _DelayMs(50 * 2);
  _WriteLcdReg(0x07,0x0033);
  _DelayMs(50 * 2);

  _WriteLcdReg(0x01,0x2B3F);
  _WriteLcdReg(0x02,0x0600);
  _WriteLcdReg(0x10,0x0000);
  _DelayMs(15 * 2);
  _WriteLcdReg(0x11,0xC5B0);  // 60B0: RGB I/R
  _DelayMs(20 * 2);
  _WriteLcdReg(0x15,0x00D0);

  _WriteLcdReg(0x05,0x0000);
  _WriteLcdReg(0x06,0x0000);
  _WriteLcdReg(0x16,0xEF1C);
  _WriteLcdReg(0x17,0x0003);
  _WriteLcdReg(0x07,0x0233);
  _WriteLcdReg(0x0B,0x5310);
  _WriteLcdReg(0x0F,0x0000);
  _WriteLcdReg(0x25,0xE000);
  _DelayMs(20 * 2);

  _WriteLcdReg(0x41,0x0000);
  _WriteLcdReg(0x42,0x0000);
  _WriteLcdReg(0x48,0x0000);
  _WriteLcdReg(0x49,0x013F);
  _WriteLcdReg(0x44,0xEF00);
  _WriteLcdReg(0x45,0x0000);
  _WriteLcdReg(0x46,0x013F);
  _WriteLcdReg(0x4A,0x0000);
  _WriteLcdReg(0x4B,0x0000);
  _DelayMs(20 * 2);

  _WriteLcdReg(0x30,0x0707);
  _WriteLcdReg(0x31,0x0600);  // 0704
  _WriteLcdReg(0x32,0x0005);  // 0204
  _WriteLcdReg(0x33,0x0402);  // 0201
  _WriteLcdReg(0x34,0x0203);
  _WriteLcdReg(0x35,0x0204);
  _WriteLcdReg(0x36,0x0204);
  _WriteLcdReg(0x37,0x0401);  // 0502
  _WriteLcdReg(0x3A,0x0302);
  _WriteLcdReg(0x3B,0x0500);
  _DelayMs(20 * 2);
  _WriteLcdReg(0x22,0x0000);
  _DelayMs(20 * 2);
}
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,057件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Sep 04 17:32:01 MST 2012
Hi Engin,
The BSP can be used with Embedded Artists 7" TFT,4.3"TFT and 3.2" QVGA LCD. 3.2" QVGA LCD need to be initialized using SPI.

I am not sure why Your code is crashing. May be you want to share your code and schematics.

Please also go to Embedded Artist's Website. Below is the link of 7" TFT. You can also look documentation for other LCDs
http://www.embeddedartists.com/products/displays/lcdb_70.php
0 件の賞賛
返信

3,057件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by e135193 on Tue Sep 04 12:57:45 MST 2012
Hello mc

   In the function below, there is a comment like "Display init sequence" Therefore I confused about the ınterface of the LCD.

   I'm sure that LCD works in 5:6:5 mode but I think that those configuration lines is not for touch chip. if those SPI interface for touch chip, then why there is a comment like "Display init sequence"   

   If you think that those lines is for touch chip, then there should be no effect when I comment out all of then. However my CPU crashes.



static void _InitTrulyLCD(void){
  
  //
  // Display init sequence
  //
  _WriteLcdReg(0x00,0x0001);
  _DelayMs(15 * 2);
  _WriteLcdReg(0x03,0x6E3E);  // AAAC
  _WriteLcdReg(0x0C,0x0007);  // 0002
  _WriteLcdReg(0x0D,0x000E);  // 000A
  _WriteLcdReg(0x0E,0x2C00);  // 2C00
  _WriteLcdReg(0x1E,0x00AE);  // 00B8 .......


}



engin
0 件の賞賛
返信

3,057件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Aug 27 09:07:03 MST 2012
Hi e135193,
SPI interface is for touch chip. LPC1788 LCD Controller directly controls LCD in 5:6:5 mode.
0 件の賞賛
返信

3,057件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by e135193 on Sat Aug 25 22:43:53 MST 2012
Helli mac

   i am not using EA's board. i am just trying to port emWin which is already ported for EA's board. What i wanted to know is that what Are these "spi" commands. Because i do not know what type of EA's LCD, i can not modify the emwin code to my LCD. That's Why i wanted to know the LCD.
0 件の賞賛
返信

3,057件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Aug 20 19:22:03 MST 2012
Hi E135193,
If you have LCD from EA you can ask schematics for LCD board from EA. Actually EA1788 BSP works with this LCD. BSP with emWin for EA1788 is at
http://www.lpcware.com/content/nxpfile/nxplpc1788emwin516bspv101.

It is not clear if you are using EA Board or not?
0 件の賞賛
返信