Duplicate variable declarations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Duplicate variable declarations

522 Views
Julian99
Contributor III

I am working on a new project using the LPC824 board and the downloaded lpcxpresso824max_new_project. It built, downloaded and debugged without problems. Initially I am trying to implement a 3-digit 7-segment LED display. I added declarations in peripherals.h and an update routine in main.c. When I build I get two errors - duplicated variable declarations. If I comment them out I get a message "undeclared variable". If I change the name of the variable I get the same duplication error. I have searched every source file in the project and cannot find any duplicates. One of the error messages is: -

/Applications/MCUXpressoIDE_25.6.136/ide/plugins/com.nxp.mcuxpresso.tools.macosx_25.6.0.202501151204/tools/bin/../lib/gcc/arm-none-eabi/14.2.1/../../../../arm-none-eabi/bin/ld: ./source/peripherals.o:/Users/julian/Documents/MCUXpressoIDE_25.6.136/workspace/lpcxpresso824max_new_project/Debug/../source/peripherals.h:57: multiple definition of `CA_LUT'; ./source/main.o:/Users/julian/Documents/MCUXpressoIDE_25.6.136/workspace/lpcxpresso824max_new_project/Debug/../source/peripherals.h:57: first defined here

 

0 Kudos
Reply
3 Replies

456 Views
Julian99
Contributor III

This is the entry in peripherals.h for both errors

// Lookup table for digits 0-9 (0 = ON, 1 = OFF)
const uint32_t CA_LUT[10] = {
//0: A, B, C, D, E, F are ON; G, DP are OFF
~((1<<SEG_A)|(1<<SEG_B)|(1<<SEG_C)|(1<<SEG_D)|(1<<SEG_E)|(1<<SEG_F)),
// 1: B, C are ON
~((1<<SEG_B)|(1<<SEG_C)),
// 2: A, B, D, E, G are ON
~((1<<SEG_A)|(1<<SEG_B)|(1<<SEG_D)|(1<<SEG_E)|(1<<SEG_G)),
// 3: A, B, C, D, G are ON
~((1<<SEG_A)|(1<<SEG_B)|(1<<SEG_C)|(1<<SEG_D)|(1<<SEG_G)),
// 4: B, C, F, G are ON
~((1<<SEG_B)|(1<<SEG_C)|(1<<SEG_F)|(1<<SEG_G)),
// 5: A, C, D, F, G are ON
~((1<<SEG_A)|(1<<SEG_C)|(1<<SEG_D)|(1<<SEG_F)|(1<<SEG_G)),
// 6: A, C, D, E, F, G are ON
~((1<<SEG_A)|(1<<SEG_C)|(1<<SEG_D)|(1<<SEG_E)|(1<<SEG_F)|(1<<SEG_G)),
// 7: A, B, C are ON
~((1<<SEG_A)|(1<<SEG_B)|(1<<SEG_C)),
// 8: All segments ON (A-G)
~((1<<SEG_A)|(1<<SEG_B)|(1<<SEG_C)|(1<<SEG_D)|(1<<SEG_E)|(1<<SEG_F)|(1<<SEG_G)),
// 9: A, B, C, D, F, G are ON
~((1<<SEG_A)|(1<<SEG_B)|(1<<SEG_C)|(1<<SEG_D)|(1<<SEG_F)|(1<<SEG_G))
};

// Global variables holding the current numbers to be printed on Digits 1, 2, and 3
volatile uint8_t display_buffer[3] = {1, 2, 3}; // E.g., displays "123"

Both errors are used in main.c :-

uint8_t numeric_value = display_buffer[current_digit];
uint32_t segment_pattern = CA_LUT[numeric_value];

#include "peripherals.h" appears only in the following files: -

main.c, peripherals.c, 

AS I mentioned I am coming over from CodeWarrior, so my knowledge of MCUX is probably dangerous (?????). I'm not sure whether a 7-segment display is a peripheral device (peripherals.h and c) or a declaration for a number of pins (pin_mux.h and c), but that can be sorted out later.

 

 

0 Kudos
Reply

449 Views
luis_maravilla
NXP Employee
NXP Employee

Hi,

It could be that, as you define CA_LUT in peripherals.h both the main and peripherals.c call that file giving the duplicate error "multiple definition".

Could you help us try to add the declaration of CA_LUT only in peripherals.c instead of peripherals.h, and retry;

Do you have more declarations as this in peripherals.h? and they have the same error? If you have them please also move them to peripherals.c

Consider your 7 segments as an external peripheral device.

Let me know your findings

Best Regards

0 Kudos
Reply

489 Views
luis_maravilla
NXP Employee
NXP Employee

Hello,

Could you please share your peripherals.h file and peripherals.c? Or describe how did you add the declaration for CA_LUT?

Could you please share how did you use CA_LUT in main.c?

Kindly share all the files names in which do you have [#include "peripherals.h"], are those files headers included in main.c?

Best Regards, Luis

0 Kudos
Reply