Driver for LCD ST7735, LPC1768/9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driver for LCD ST7735, LPC1768/9

2,511 Views
senersoft
Contributor I

Hi,

I have a LCD driver for a LPC1768 or (LPC1769) device. It works somehow. But, it is far from being efficient, it is slow. Even though I played with SPI speed from 1Mhz up to 25Mhz, it didn't make any difference. Do you know this is something known? Or is there a decent LCD driver for ST7735 ported to LPC17xx?

Thank you.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

2,435 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi, I hope you're doing well!

 

I'm sorry for the inconveniences this may cause, but there's currently no driver available specifically for connecting the ST7735 LCD Display and an LPC1768/9.

It seems like it could be a limitation of the LCD, as changing the SPI speed seems to not affect the LCD's performance.

Please let me know if you need any more information.

 

Take care, best regards,

Sebastian

0 Kudos
Reply