Driver Doubt ADC - LPC55S16

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Driver Doubt ADC - LPC55S16

2,140 次查看
Dhayanandhan
Contributor I

We are customizing ADC channel in LPC 55S16 to use multiple channel

Here we are using following pins

P1_9 (ADC0_12), P1_8(ADC0_4),  P0_16(ADC0_8)   )

How we can configure multiple channels for those pins

i) Is any relation between ADC channel and SWTRIG

 How we can choose the value of ADC0->SWTRIG = ?

ii) Is any relation between TCTRL and SWTRIG

 How we can choose the element and value of  of ADC0->TCTRL[?] = ?

Kindly give the solution to solve the problem

0 项奖励
回复
5 回复数

2,124 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The LPC55ss ADC support command chain, each command register includes the ADC channel, and Next Command bit field which point to next command.

In the first command, you can define the ADC channel, in the next command bit field, you can set up the chained command index. In the chained command, you can define the second ADC channel and secondly chained next-command. In the secondly-chained command register, you can define the third ADC analog channel, if this is the last channel, set the third-chained next-command bits as 0, which means chaining ends up.

The following is the command chain, hope it can help you.

lpadc_conv_command_config_t mLpadcCommandConfigStruct0,mLpadcCommandConfigStruct1,mLpadcCommandConfigStruct2;

 

LPADC_GetDefaultConvCommandConfig(&mLpadcCommandConfigStruct0);

    mLpadcCommandConfigStruct0.channelNumber = DEMO_LPADC_USER_CHANNEL; //adc channel0

    mLpadcCommandConfigStruct0.chainedNextCommandNumber=DEMO_LPADC_USER_CMDID2;

    LPADC_SetConvCommandConfig(DEMO_LPADC_BASE, DEMO_LPADC_USER_CMDID1, &mLpadcCommandConfigStruct0);

 

    ///////////////Rong added another adc channel

    LPADC_GetDefaultConvCommandConfig(&mLpadcCommandConfigStruct1);

    mLpadcCommandConfigStruct1.channelNumber = DEMO_LPADC_USER_CHANNEL+1;  //DEMO_LPADC_USER_CHANNEL+1=1, adc channel1

    mLpadcCommandConfigStruct1.chainedNextCommandNumber=DEMO_LPADC_USER_CMDID3;

    LPADC_SetConvCommandConfig(DEMO_LPADC_BASE, DEMO_LPADC_USER_CMDID2, &mLpadcCommandConfigStruct1);

 

    LPADC_GetDefaultConvCommandConfig(&mLpadcCommandConfigStruct2);

    mLpadcCommandConfigStruct2.channelNumber = DEMO_LPADC_USER_CHANNEL+2;  //DEMO_LPADC_USER_CHANNEL+1=1, adc channel1

    mLpadcCommandConfigStruct2.chainedNextCommandNumber=0;

    LPADC_SetConvCommandConfig(DEMO_LPADC_BASE, DEMO_LPADC_USER_CMDID3, &mLpadcCommandConfigStruct2);

 hope it can help you.

BR

XiangJun Rong

 

 

0 项奖励
回复

2,089 次查看
Dhayanandhan
Contributor I

Thanks for the support.

could you help me to configure ADC for channel 8 (i.e, ADC0_8     P0_16)

Kindly forward the ADC driver to configuring ADC0_8

0 项奖励
回复

2,135 次查看
Dhayanandhan
Contributor I

I need to configure ADC for these PINS

P1_9 (ADC0_12), P1_8(ADC0_4),  P0_16(ADC0_8)  

0 项奖励
回复

2,072 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the P1_9 (ADC0_12), it's channel index is CH4B. For the P1_8(ADC0_4), it's channel index is CH4A.

If you sample P1_9 (ADC0_12, CH4B), you can use the code:

LPADC_GetDefaultConvCommandConfig(&mLpadcCommandConfigStruct1);

mLpadcCommandConfigStruct1.sampleChannelMode=kLPADC_SampleChannelSingleEndSideB;

    mLpadcCommandConfigStruct1.channelNumber = 4;  //CH4A

    mLpadcCommandConfigStruct1.chainedNextCommandNumber=DEMO_LPADC_USER_CMDID3;

    LPADC_SetConvCommandConfig(DEMO_LPADC_BASE, DEMO_LPADC_USER_CMDID2, &mLpadcCommandConfigStruct1);

 

If you sample P1_8(ADC0_12, CH4A), you can use the code:

LPADC_GetDefaultConvCommandConfig(&mLpadcCommandConfigStruct1);

mLpadcCommandConfigStruct1.sampleChannelMode=kLPADC_SampleChannelSingleEndSideA;

    mLpadcCommandConfigStruct1.channelNumber = 4;  //CH4A

    mLpadcCommandConfigStruct1.chainedNextCommandNumber=DEMO_LPADC_USER_CMDID3;

    LPADC_SetConvCommandConfig(DEMO_LPADC_BASE, DEMO_LPADC_USER_CMDID2, &mLpadcCommandConfigStruct1);

Hope it can help you

BR

XiangJun Rong

2,055 次查看
Dhayanandhan
Contributor I

could you help me to configure ADC for channel 8 (i.e, ADC0_8 ,   PIN P0_16)

0 项奖励
回复