Does not MCU-Link support LPC2168?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does not MCU-Link support LPC2168?

Jump to solution
1,680 Views
andy_
Contributor I

Hi. I was about to place an order for MCU-Link or MCU-Link Pro to work on a LPC2168 based board but I have just noticed that LPC2168 is not available in the supported device list. Is there an error or am I missing something? With a quick search, I see that LPC-Link2 supports LPC2138. But it is unavailable or obsolete. What should I get to work on LPC2138? Thanks.

Labels (2)
0 Kudos
Reply
1 Solution
1,642 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @andy_ 

The LPC2168  is quite old.

For MCU LINK, we have only tested the listed devices.

You can try to visit the Keil official website.

NXP (founded by Philips) LPC2148

BR

Harry

View solution in original post

0 Kudos
Reply
1 Reply
1,643 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @andy_ 

The LPC2168  is quite old.

For MCU LINK, we have only tested the listed devices.

You can try to visit the Keil official website.

NXP (founded by Philips) LPC2148

BR

Harry

0 Kudos
Reply