Does any microcontroller in LPC series has inbuilt capacitive touch peripheral?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does any microcontroller in LPC series has inbuilt capacitive touch peripheral?

1,544 Views
chromeankit
Contributor I

Looking for inbuilt capacitive touch peripheral in LPC series microcontroller.

Tags (1)
0 Kudos
Reply
1 Reply

1,356 Views
soledad
NXP Employee
NXP Employee

Hi,

At this moment, we only can suggest the below links, I hope this helps.

AN11023: Capacitive touch sensing using the LPC11xx (with software) (v.1.0) | www.LPCware.com 

AN11095: Capacitive touch sensing using the LPC176x/5x | www.LPCware.com 

LPC82x Touch Solution|NXP 

Proximity Capacitive Touch Sensor Controller|NXP 

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply