Does a Unique ID exists for a LPC18S37?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does a Unique ID exists for a LPC18S37?

2,095件の閲覧回数
nxp68994
NXP Employee
NXP Employee

The user manual for the LPC18S37 (UM10430) list the feature on page 14:

Unique ID for each device.
But the Unique ID is never referenced in the entire manual. My question: does a Unique ID exist in ROM code of the LPC18S37 which can be used a serial number?

Thanks

0 件の賞賛
返信
3 返答(返信)

1,968件の閲覧回数
nxp68994
NXP Employee
NXP Employee

Hi Jeremyzhou,

I found it at “5.7.13 Read device serial number”.

Thank you!

0 件の賞賛
返信

1,968件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Wolfgang Kramper,

Welcome.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,968件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Wolfgang Kramper,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

Q1) My question: does a Unique ID exist in ROM code of the LPC18S37 which can be used a serial number?

-- No, you can read the unique part ID by referring to Fig 1.

pastedImage_2.png

Fig 1


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信