Does a Unique ID exists for a LPC18S37?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does a Unique ID exists for a LPC18S37?

2,108 Views
nxp68994
NXP Employee
NXP Employee

The user manual for the LPC18S37 (UM10430) list the feature on page 14:

Unique ID for each device.
But the Unique ID is never referenced in the entire manual. My question: does a Unique ID exist in ROM code of the LPC18S37 which can be used a serial number?

Thanks

0 Kudos
Reply
3 Replies

1,981 Views
nxp68994
NXP Employee
NXP Employee

Hi Jeremyzhou,

I found it at “5.7.13 Read device serial number”.

Thank you!

0 Kudos
Reply

1,981 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Wolfgang Kramper,

Welcome.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,981 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Wolfgang Kramper,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

Q1) My question: does a Unique ID exist in ROM code of the LPC18S37 which can be used a serial number?

-- No, you can read the unique part ID by referring to Fig 1.

pastedImage_2.png

Fig 1


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply