Does NXP plan to have ULPI support (External HS PHY) for the LPC546XX family ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does NXP plan to have ULPI support (External HS PHY) for the LPC546XX family ?

1,581件の閲覧回数
k2
Contributor III

NXP support,

I'm wondering if you have any plans to add ULPI to the LPC546XX family ?

I have a working LPC4337 ULPI design with DUAL HS USB ports, but would like to see

this interface in the LPC546XX family as it's better supported in MCU Expresso.

Kevin 

ラベル(5)
0 件の賞賛
返信
1 返信

1,399件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Kevin King,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

I think the LPC546xx series willn't release some particular chips which supports extrnal ULPI PHY in future, as the LPC546xx series contains on-chip high-speed UTMI+ compliant PHY.

Hope this is clear.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信