Does LPC1769 Support 10-bit addressing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does LPC1769 Support 10-bit addressing

1,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vinay singh on Thu Apr 24 01:43:37 MST 2014
Hello.
Need urgent information if I2C peripheral on LPC1769 support a 10-bit slave addressing mode.
When LPC1769 is configured as I2C slave does it respond to a 10-bit address when issued by the master, if it does then please let me know the procedure as to how it is done, some example code would be helpful.

Anyone please respond as i need a solution urgently..

Thanks in Advance.


Thanks and Regards,
Vinay Singh
ラベル(1)
0 件の賞賛
返信
1 返信

1,042件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Wed Apr 30 11:06:50 MST 2014
Hi Vinay,

LPC1769 I2C peripheral does not support 10-bit addressing.


Thanks,

NXP Technical Support
0 件の賞賛
返信