Display goes Gray and Blur on creation of the Graph Widget

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Display goes Gray and Blur on creation of the Graph Widget

868件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PrasadT10 on Tue May 24 23:32:13 MST 2016
Hi, In one of the screens, we are trying to create a Graph.

{ GRAPH_CreateIndirect, "Graph", ID_GRAPH_0,    1,  45, 318, 140, 0, 0x0, 0 },

Just when the initialization is done, the whole screen goes Gray and gets blurred until I reset the unit.Initialization of the Graph widget in WM_INIT_DIALOG:
hItem = WM_GetDialogItem(pMsg->hWin, ID_GRAPH_0);

GRAPH_SetBorder(hItem, 40, 1, 1, 30);
hData = GRAPH_DATA_YT_Create(GUI_DARKGREEN, 500, 0, 0);
GRAPH_AttachData(hItem, hData);
GRAPH_SetGridDistY(hItem, 25);
GRAPH_SetGridVis(hItem, 1);
GRAPH_SetGridFixedX (hItem, 1);
hScaleV = GRAPH_SCALE_Create(35, GUI_TA_RIGHT, GRAPH_SCALE_CF_VERTICAL, 25);
#ifdef USE_FONTS
GRAPH_SCALE_SetFont(hScaleV, FONT_CALIB16);
#endif
GRAPH_AttachScale(hItem, hScaleV);
hScaleH = GRAPH_SCALE_Create(110, GUI_TA_HCENTER, GRAPH_SCALE_CF_HORIZONTAL, 50);
#ifdef USE_FONTS
GRAPH_SCALE_SetFont(hScaleH, FONT_CALIB16);
#endif
GRAPH_AttachScale(hItem, hScaleH);
GRAPH_SetColor(hItem, Custom_Color, GRAPH_CI_BORDER);
GRAPH_SetUserDraw(hItem, _UserDraw);

We are drawing a Rect on the screen and the graph is drawn in the rect.
Part of the GUI_PAINT looks something like this:
GUI_SetBkColor(Custom_Color);

GUI_SetColor(Custom_TextColor);
GUI_Clear();
GUI_DrawRect(0, 0, (FB_XSIZE-1), (FB_YSIZE-1));
GUI_DrawHLine(40, 0, FB_XSIZE);
GUI_DrawHLine(190, 0, FB_XSIZE);
To my surprise, if I comment out the GUI_SetBkColor() from the WM_PAINT event, the graph is displayed with properties set by me, but the rest of the screen is still Gray, but not blurred out.

Have anybody come across such a situation? What might have caused this?
ラベル(1)
0 件の賞賛
返信
1 返信

745件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信