Diolan LPC-4350-DB1 development board SD example??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Diolan LPC-4350-DB1 development board SD example??

1,086件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by picman on Thu Feb 07 01:41:43 MST 2013
Has anyone managed to get the SD interface working on the Diolan  LPC-4350-DB1 development board?

I think mine has the rev A chip, does the SD interface work with this chip?


Thanks
Nick
ラベル(1)
0 件の賞賛
返信
1 返信

1,066件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Thu Feb 07 10:33:16 MST 2013
Hello Nick,

the chip has no problem with the SD card interface. Maybe it's just a pin multiplexing issue.

In the KEIL µVision environment there is an example from KEIL for the SD card (go to the folder "\Keil\ARM\Boards\Keil\MCB4300\RL\FlashFS\SD_File" of the µVision installation).

In our LPCOpen platform ( http://lpcware.com/content/nxpfile/lpcopen-platform  ) there is also an example for it (go to the folder "\lpcopen\applications\lpc18xx_43xx\examples\periph\periph_sdmmc")

Maybe this gives you an idea what's required to make it working on the Diolan board.

Best regards,
Bernhard.
0 件の賞賛
返信