Difference between debug, release builds

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between debug, release builds

ソリューションへジャンプ
1,861件の閲覧回数
YaronAlexandrovich
Contributor V

There are four scenarios:

Run a debug session using the 'PE Debug' build

Run a board that has been flashed with a 'PE Debug' build, not in debugger

Run a debug session using the 'PE Release' build  

Run a board that has been flashed with a 'PE Release' build, not in debugger

 

I know RTFM is the right answer here, but I would appreciate a brief explanation of what is occurring in each of these 4 scenarios, as each leads to different behaviors.  
Also, to prove code correctness, I assume the code should work properly under a 'PE Release' non-debug session.  As of now only a 'PE Debug' debug session works correctly.  

0 件の賞賛
返信
1 解決策
1,837件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @YaronAlexandrovich 

Do you mean MCUXpresso IDE? If yes, please see <MCUXpresso_IDE_User_Guide.pdf>

MCUXpresso IDE creates projects with two build configurations, Debug and Release (but you can also add more if required). These differ in the default level of compiler optimization.
Debug projects default to None (-O0), and Release projects default to (-Os). For more information
on switching between build configurations, see How do I switch between Debug and Release
builds? 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,838件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @YaronAlexandrovich 

Do you mean MCUXpresso IDE? If yes, please see <MCUXpresso_IDE_User_Guide.pdf>

MCUXpresso IDE creates projects with two build configurations, Debug and Release (but you can also add more if required). These differ in the default level of compiler optimization.
Debug projects default to None (-O0), and Release projects default to (-Os). For more information
on switching between build configurations, see How do I switch between Debug and Release
builds? 

BR

Alice

0 件の賞賛
返信