Difference between LPC Open and Library from lpcware git

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between LPC Open and Library from lpcware git

861件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by amoehl on Mon Apr 15 02:55:26 MST 2013

Hello,


i am a little confused. Meanwhile i have two different libraries. One comes with Code Red Suite in the Example and is also here in the git:


http://git.lpcware.com//lpc43xx


The other is the lpcOpen.


It seems, that booth are made from NXP, but the name scheme and the folder structure are complete different. Currently i use the Lib from the git above.
But when i tried to use the USB Example, it doesn't work. So i tried to use the USB lib from lpcopen but this needs the


 


So, what should i use?? What are the Pro's and the Con's for the libraries?


Regards,


Andre

ラベル(1)
0 件の賞賛
返信
0 返答(返信)