Difference between LPC Open and Library from lpcware git

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between LPC Open and Library from lpcware git

865 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by amoehl on Mon Apr 15 02:55:26 MST 2013

Hello,


i am a little confused. Meanwhile i have two different libraries. One comes with Code Red Suite in the Example and is also here in the git:


http://git.lpcware.com//lpc43xx


The other is the lpcOpen.


It seems, that booth are made from NXP, but the name scheme and the folder structure are complete different. Currently i use the Lib from the git above.
But when i tried to use the USB Example, it doesn't work. So i tried to use the USB lib from lpcopen but this needs the


 


So, what should i use?? What are the Pro's and the Con's for the libraries?


Regards,


Andre

标签 (1)
0 项奖励
回复
0 回复数