Device could not be powered up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device could not be powered up

2,871 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LPC54102 on Fri Jun 12 02:33:12 MST 2015
Hello,

as debugger i´m using keil ULINK2.
Microcontroller: LPC54102

Problem:
I can´t erase or debug the microcontroller. I get the message "Device could not be powered up".

How do I get a connection to the microcontroller?
Labels (1)
0 Kudos
Reply
2 Replies

2,425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Wed Jul 01 15:05:24 MST 2015
Hi LPC54102,

What IDE are you using? Please try to put the MCU into ISP mode and see if the debugger can connect to the MCU.
0 Kudos
Reply

2,425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OldisGold on Wed Jun 17 11:49:31 MST 2015
If you are using windows 8.1check USB power settings on your host computer.

Or try using a powered usb hub.

0 Kudos
Reply