Device could not be powered up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device could not be powered up

2,933件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LPC54102 on Fri Jun 12 02:33:12 MST 2015
Hello,

as debugger i´m using keil ULINK2.
Microcontroller: LPC54102

Problem:
I can´t erase or debug the microcontroller. I get the message "Device could not be powered up".

How do I get a connection to the microcontroller?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,487件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Wed Jul 01 15:05:24 MST 2015
Hi LPC54102,

What IDE are you using? Please try to put the MCU into ISP mode and see if the debugger can connect to the MCU.
0 件の賞賛
返信

2,487件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OldisGold on Wed Jun 17 11:49:31 MST 2015
If you are using windows 8.1check USB power settings on your host computer.

Or try using a powered usb hub.

0 件の賞賛
返信